Technical FAQs

Ask a Question

What is the difference between LCSBasic and LCSAdvanced?

What is the difference between LCSBasic and LCSAdvanced?

Product Line:
Powerlink Lighting Control
Powerlink G3

North America, Commercial Building

Product Selection

LCSBasic and LCSAdvanced are similar in most respects.  There are 2 major differences.  

The first major difference is that LCSAdvanced allows multiple Powerlink Devices to be part of a "system".    One can go online with the system and be connected to all of Powerlink Devices at the same time.   This is useful if the Powerlink application is a building with multiple panels all on the same LAN, administered from a central control station.   LCSBasic only allows one device per system.  If one had multiple controllers, one must save each one as a separate system, connect to one Powerlink Controller at a time.  

The other difference between LCSAdvancedand LCSBasic is that LCSAvanced has a Device Discovery function.   One can input a range of serial address or IP Addresses and let the software search for Powerlink Controllers on the network.  

Catalog Pages are attached.
Was this helpful?
What can we do to improve the information ?