Technical FAQs

Ask a Question

Can you order an input line reactor for the enclosed S-Flex ATV212 drives?

Issue:
Can you order an input line reactor for the enclosed S-Flex ATV212 drives?

Product Line:
Altivar 212 S-Flex

Environment:
All S-flex 212 drives with the Mod X07 installed from the factory.

Cause:
Needs to know if they can order a input line reactor with the enclosed S-flex drives and what is the line reactor impedance size?

Resolution:
Yes you can order an input line reactor modification under Mod X07.
Please note the X07 mod will have 1.5% line impedance.
Was this helpful?
What can we do to improve the information ?