Technical FAQs

Ask a Question

Is the RQC150SFMG provided with a factory installed service disconnect?

Issue:
Application

Product Line:
CSED

Environment:
Application

Cause:
Clarification

Resolution:
Yes, the 150A service disconnect is factory installed device. The main breaker is catalog number QOM2150VH.


CTA-ID : 2030577
Was this helpful?
What can we do to improve the information ?