Technical FAQs

Ask a Question

Is the RC200SFMG provided with a factory installed service disconnect?

Issue:
Application

Product Line:
CSED

Environment:
Application

Cause:
Clarification

Resolution:
No, the service disconnect must be field installed in this device. Install only QOM2-VH type of breaker, 200 ampere maximum.


CTA-ID : 2030577
Was this helpful?
What can we do to improve the information ?