Technical FAQs

Ask a Question

Will a QO120DF (Dual Function CAFI-GFI) breaker, work in a Plug-On Neutral style QO Load center ?


Issue:
Will a QO120DF (Dual Function) breaker, work in a Plug On Neutral style QO Load center ?

Product Line:
QO Load Center

Environment:
Installation

Cause:
Clarification
 
Resolution:

Yes, it will work in the newer PON (Plug On Neutral) load centers. The Plug On Neutral load centers also accept QO120PDF, which would not have the pigtail.
Was this helpful?
What can we do to improve the information ?