Technical FAQs

Ask a Question

What is the Schneider recommended part number for an output filter for a 60 horsepower, 460 volts motor?

Issue:
,What is the Schneider recommended part number for an output filter for a 60 horsepower 460 volts motor?

Product Line:
ALTIVAR 61/71

Environment:
60 HP/ 460 volts output filters

Cause:
1 - Product Selection & Services

Resolution:
KLCUL80A2
Was this helpful?
What can we do to improve the information ?