Technical FAQs

Ask a Question

What are the available condiut entries for a XCKD, XCKP, or XCKT limit switch?

Issue:
Identifying characteristics from part numbers

Product Line:
XCKD, XCKD, XCKT limit switches
ZCD, ZCP, ZCT limit switches

Environment:
US Product

Cause:
It is necessary to have the appropiate conduit entry on a limit switch

Resolution:
For a complete limit switch (XC devices) use the following suffixes:
P16 - ISO M16
P20 - ISO M20
G11 - Pg11
G13 - PG 13.5
N12 - 1/2" NPT
F12 - PF 1/2" NPSF
D44 - Deutch Connector

For the adapter to fit with a metallic limit switch body (ZCD devices) order the following pieces:
ZCDEP16 - ISO M16
ZCDEP20 - ISO M20
ZCDEG11 - Pg11
ZCDEG13 - PG 13.5
ZCDEN12 - 1/2" NPT
ZCDEF12 - PF 1/2" NPSF

For the adapter to fit with a plastic limit switch body (ZCP, ZCT devices) order the following pieces:
ZCPEP16 - ISO M16
ZCPEP20 - ISO M20
ZCPEG11 - Pg11
ZCPEG13 - PG 13.5
ZCPEN12 - 1/2" NPT
ZCPEF12 - PF 1/2" NPSF
ZCPED44 - Deutch Connector

 

Was this helpful?
What can we do to improve the information ?