Technical FAQs

Ask a Question

Is the XALD101H29H7 available with special markings instead of "start" ?

Issue:
Is the XALD101H29H7 available with special  engravings or markings instead of "START" ? 

Product Line:
XALD 22mm control station

Environment:
XAL, 22mm control stations  and enclosures

Cause:
Special engraving requested

Resolution
You must purchase the components separate.  order as  a  XALD01H7 push button enclosure ,  XB5AA61  push button and a custom  legend part number ZBY2002 and specify the required engraving
Was this helpful?
What can we do to improve the information ?