Technical FAQs

Ask a Question

ATV71 what is the default settings for Otrn Int (units), if devicenet is not used?

Issue:
Using an ATV71 and canopen can not program parameter code Otrn (Int).

Product Line:
ALTIVAR 71

Environment:
All
 
Cause:

11 - Additional Documentation Request

Resolution:
What are the default torque unit settings for parameter code Otrn, if devicenet is not used?
The default units will be :
- For ATV71 of size 0,37 ...75Kw  --> INT=1 [means  0.1Nm]
- For the ATV71 of size  > 75Kw  -->  INT=2 [means: 1Nm   ]

 
Was this helpful?
What can we do to improve the information ?