Technical FAQs

Ask a Question

Are alternate lugs available for the EZM3800TBCU Main device?

ISSUE:
Alternate Lugs

PRODUCT LINE:
EZM Metering

ENVIRONMENT:
Alternate Lugs

CAUSE:
Change in Wire Size

RESOLUTION:
The standard terminal lug data for the EZM3800TBCU is (4) 3/0 - 500kcmil Al/Cu wires per phase and neutral and (1) #6 - 300kcmil Al/Cu for the ground lug.

To use (2) 1/0 - 600 kcmil Al/Cu wires Max. per phase and neutral or (4) 1/0 - 250 kcmil Al/Cu wires Max per Phase and Neutral use the mechanical lug kit MMLK250.
The kit inlcudes 3 double barrel lugs and each lug will accept (1) 600kcmil or (2) 250kcmil wires, then each phase and the neutral will accept 2 Lugs.The ground lug remains the same as the above standard.
 


 
Was this helpful?
What can we do to improve the information ?