Technical FAQs

Ask a Question

Altering head position on XCMN limit switches

Issue:
Can the orientation of the head be adjusted on an XCMN limit switch, for example can it be removed, rotated 90 degrees, and reinserted as with the XCMD units?

Product Line:
XCMN limit switches

Environment:
US Product

Cause:
There is little documentation on these units

Resolution:
These units cannot be field modified.  The head is locked into position with two pins which cannot be removed.
 
Was this helpful?
What can we do to improve the information ?