Technical FAQs

Ask a Question

The ATS01 LY high HP soft starters are now obsolete what is the recommended replacement?

Issue:
The ATS01 LY high HP soft starters are now obsolete what is the recommended replacement?

Product Line:
Altistart ATS01 LY only

Environment:
All

Cause:
The ATS01 LY is now obsolete and the end customer needs a similar replacement unit.

Resolution:
The ATS01 is obsolete however if you nee a similar replacement unit you might want to look at the ATS22 family.  Choose new ATS22 based on your application like HP, Voltage and motor current.
See the attached ATS22 Manual.


 
Was this helpful?
What can we do to improve the information ?