Technical FAQs

Ask a Question

What is the standard operating temperature range of a 9070 type T or TF control transformer?

Issue:
CPT Operating temperature

Product Line:
Control Power Transformer

Environment:
9070T and 9070TF

Cause:
Application

Resolution:
The 9070 Type T or TF control transformer is designed to operate in a -40degC to +40degC (-40degF to +104degF) ambient. However, the 24 hour average ambient should not exceed 30degC (86degF.)



 
Was this helpful?
What can we do to improve the information ?