Technical FAQs

Ask a Question

What are the repair parts for an EZMR113225CUX, Series M03 branch unit?

Issue:
Repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:

Customer Cover (includes labels) - EZM113225C
Cover Screws - 4020513002K
Meter Socket Cover (cover for one meter position) - MMRC
Spacer Cover above top meter cover position - EZM23TBKC
Parts Kit (one position, meter socket line side through tenant breaker base) - EZM1225KIT
Circuit Breaker RB Cover (one position) - BCV
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329772401
Branch Neutral Lug assembly - 7329752253 (includes 3 lugs and the bus bar the lugs are mounted to)
Mounting screws and washer for Branch neutral lug assembly - 2159417241(1-screw required), 2159417121(1-screw required) and 2390331201(1-washer required)
Equipment Ground lug assembly - 7329897052 (includes 3 lugs and the mounting bracket)
Equipment Ground lug assembly mounting Screws - (2) 2142217101    
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP


 
Was this helpful?
What can we do to improve the information ?