Technical FAQs

Ask a Question

Available Coil Voltages for 8965RO contactors

Issue:

What coil voltages are available for the 8965RO reversing contactor?

Product Line:

8965RO Reversing Definite Purpose Contactors

Environment:

US Product

Cause:

Information for these contactors is scarce

Resolution:

V01 - 24Vac
V02 - 120Vac
V21 - 208/220Vac
V03 - 240Vac
V06 - 480Vac
V07 - 600Vac

**As of 1/01/2015 only the V01 (24Vac) and V02 (120Vac) are available.  All other options have been obsoleted**
 

Was this helpful?
What can we do to improve the information ?