Technical FAQs

Ask a Question

What is the wire size for 8910DPA93V02?

ISSUE:
What is the wire size for 8910DPA93V02

PRODUCT LINE:
8910 Definite Purpose Contactors

ENVIRONMENT: 
8910 DP contactors, 90A

CAUSE:
The needs The need to know wire size for installation


RESOLUTION:
The power terminals will accept (1) copper or stranded copper wire only, #14 - 1/0 awg.




KEYWORD: cable size, wire data, wire size
Was this helpful?
What can we do to improve the information ?