Technical FAQs

Ask a Question

What tenant breakers were used with the MP422R ?

Issue:
Application

Product Line:
MP Meter-Pak

Environment:
Application

Cause:
Selection

Resolution:
The MP422R accepted Q2M (10Kaic), Q2M-VH (22Kaic) or Q2MH (42Kaic) tenant breakers, 200A maximum. Example catalog number: Q2M2200
Was this helpful?
What can we do to improve the information ?