Technical FAQs

Ask a Question

For the part number XB5KSG do we need to order contacts as well?

 

Issue:
For the part number XB5KSG do we need to order contacts as well?

Product Line:
XB5 22 mm push buttons

Environment:
Products sold and used in the United States

Cause:
Selecting the complete XB5 annunciator
 
Resolution:

You do not need to order contact blocks, this is a complete device.

Was this helpful?
What can we do to improve the information ?