Technical FAQs

Ask a Question

9007T10 limit switch body

Issue:

Which standard bodies can utilize the 9007T10 head

Product Line:

9007C limit switches

Environment:

US Product

Cause:

This head can only be used with select bodies

Resolution:

The 9007T10 must be paired with a neutral position body to work properly.  The 9007CO68 and 9007CT62 can be paired together to make the correct standard box body for this switch, or the head and body can be ordered together as a 9007C68T10.

Was this helpful?
What can we do to improve the information ?