Technical FAQs

Ask a Question

Voltage for the 9999SP2, 9999SP3, 9999SP4, or 9999SP5

What voltage coil is needed for the standard pilot light kits, part numbers:
9999SP2, 9999SP2R
9999SP3, 9999SP3R
9999SP4, 9999SP4R
9999SP5, 9999SP5R

Product Line:
NEMA contactor/starter accessories

Pilot light wiring/application 

The needed voltage is not listed for these units

These pilot light kits are not powered directly by the control voltage of the contactor/starter.  They are powered by an induction coil which is supplied with the kit.  As such, they can be used with any control voltage.
Was this helpful?
What can we do to improve the information ?