Technical FAQs

Ask a Question

Mounting bracket for 9012G pressure switches

Issue:

Is there a mounting bracket available for 9012G switches?

Product Line:

9012G Industrial Pressure Switches

Environment:

US Product

Cause:

Switches may need to be mounted in locations where the standard mounting holes are not usable.

Resolution:

Some of the 9012G switches can be ordered with an alternate back which has different mounting holes.  One would need to use form F to gain this backing on a standard switch.  This option is only available on select models and cannot be ordered separately.  Dimensions are attached.

Was this helpful?
What can we do to improve the information ?