Technical FAQs

Ask a Question

What was the DO1 suffix on the ATV16 drives?

Issue:
What was the DO1 suffix on the ATV16 drives?

Product Line:
Altivar ATV16

Environment:
All

Cause:
Needs to get a replacement drive for the ATV16........D01 drive for a Crane application.

Resolution:
D01: What does D01 on the end of the Altivar ATV16 indicate?
It is a drive with special software sold only to a specific company for crane control. The company is Kone Crane and can contact them 
 

 
Was this helpful?
What can we do to improve the information ?