Technical FAQs

Ask a Question

What is the maximum number of circuits in a single tub 600a main breaker NQ 1ph panel ?

Issue:
Branch breaker count
 
Product Line:
Panelboards
 
Environment:
NQ
 
Cause:
Product features
 
Resolution:
 
 
 
 
The factory assembled panel with an LD main breaker can be provided with 84 circuits max.
 
Was this helpful?
What can we do to improve the information ?