Technical FAQs

Ask a Question

Ordering an XY2CH cable pull switch with two normally closed contacts

Issue:

How can I order an XY2CH cable pull switch with two normally closed contacts instead of one normally open and one normally closed?

Product Line:

XY2CH cable pull switches

Environment:

US Product

Cause:

Occasionally two NC contacts are needed in an application instead of a single.

Resolution:

Change the  9th digit in the part number to a 7.

Example:
XY2CH13150H7 has 1 NO and 1 NC contact
XY2CH13170H7 has 2 NC contacts

Was this helpful?
What can we do to improve the information ?