Technical FAQs

Ask a Question

What is the part number for the DC choke for an ATV61HC22N4?

Issue:
What is the part number for the DC choke for an ATV61HC22N4?

Product Line:
ATV61, ATV71

Environment:
All serial numbers for ATV61 and ATV71 90Kw/125 HP and greater at 460 volts

Cause:
Replacement DC chokes

Resolution:
The part number for the DC choke for VFDS 90kW125 HP @ 460 volts and higher is VW3A4521, however, the DC choke is only available for purchase by Schneider Services.
Was this helpful?
What can we do to improve the information ?