Technical FAQs

Ask a Question

5W lights for XVE tower lights

Issue:

Which are the 5W incandescent lights to be used with the XVE series of tower lights?

Product Line:

XVE 70mm diameter tower lights.

Environment:

US Product

Cause:

Lamps are needed to make a complete light

Resolution:

The following bulbs are available:

DL1BEBS - 4W, 24Vac/Vdc
DL1EDGS - 5W, 120Vac/Vdc
DL1BEMS - 5W, 230Vac/Vdc
 

Was this helpful?
What can we do to improve the information ?