Technical FAQs

Ask a Question

Are optional lugs available for the HU265DS Series E5 (E05), to accept up to (3) 500 KCMIL conductors per phase?

Issue:
Optional Lugs
 
Product Line:
Heavy Duty Safety Switches

Environment:
Application

Cause:
Optional lugs required for three conductors per phase

Resolution:
The standard lugs provided on the 400A Heavy Duty Safety Switch will accept up to (1) #1/0 AWG - 600 KCMIL or (2) #1/0 AWG - 300 KCMIL AL/CU conductors per phase. No alternate lugs are available to accept (3) conductors per phase.

 
Was this helpful?
What can we do to improve the information ?