Technical FAQs

Ask a Question

Replacement coils for an 8903SP lighting contactor

Issue:
What is the part number for a replacement coil for an 8903SP lighting contactor?

Product Line:
8903 lighting contactors 60A

Environment:
Maintenance

Cause:
Replacement/repair 

Resolution:
Use the attached table to specify the appropiate coil based on number of poles, voltage, and hertz.
EG. a 120V 60hz coil for a three pole unit would be 31063-409-38
Was this helpful?
What can we do to improve the information ?