Technical FAQs

Ask a Question

Can we use one of the 9999RR04 remote reset modules to control multiple 9065 solid state overload relays?

 
Issue:  Can we use one of the 9999RR04 remote reset modules on multiple 9065 solid state overload relays?    

<br /><br /> 
Product Line:
9065 solid state overload relays
<br /><br /> 
Environment:
Products sold and used in the United States
<br /><br /> 
Cause:
With multiple starters in the box they would like to use one remote reset module on multiple SSOLRs
<br /> <br /> 
Resolution:
We cannot use one remote reset module on multiple solid state overload relays. While the remote reset is electrically controlled, it mechanically actuates the reset on the solid state overload relay.
We can use one push button, with multiple contact blocks, to control the remote reset module though.

 
Was this helpful?
What can we do to improve the information ?