Technical FAQs

Ask a Question

Travel distance for plunger style 9007MS limit switches

Issue:

What is the travel distance for 9007MS plunger limit switches

Product Line:

9007MS limit switches with plunger head:

9007MS01
9007MS02
9007MS03
9007MS06
9007MS07
9007MS08
9007MS09

Environment:

US Product

Cause:

Travel distance is an important consideration for selecting limit switches for certain

Resolution:

The travel distance to engage the contacts is 0.07" and the dstance to reset the contacts is 0.004" in the opposite direction.  Total travel for these switches is limited to 0.19" and any movement beyond this distance could damage the switch.
 

Was this helpful?
What can we do to improve the information ?