Technical FAQs

Ask a Question

What does the “cc” represent in the HVL/cc product line?

The “cc” stands for Compact Compartmentalized. Reliability and performance are the primary goals of switchgear in any switching, control or protective application. We’ve taken these goals further with HVL/cc medium voltage metal-enclosed switchgear. The major differentiating features of HVL/cc switchgear are:
Compact Size – Approximately ¼ the size of traditional medium voltage metal-enclosed switchgear.
Compartmentalized Construction – The fuse/cable compartment is isolated from the main bus, while the main switch contact are housed in a sealed interrupter.
Click on the below link for more information.
Square D – HVL/cc
Was this helpful?
What can we do to improve the information ?