Technical FAQs

Ask a Question

Are PK**GTA ground bars UL508A listed?

Issue:
Are PK**GTA  ground bars UL508A listed

Product Line:
Ground bars

Environment:
UL Classification 

Cause:
If ground bar kits are UL508A listed

Resolution:
No these kits are not UL508A listed. They are UL Recognized Components - Panelboard Accessories, listed in File E6294, Volume 7, Section 31. 
Was this helpful?
What can we do to improve the information ?