Technical FAQs

Ask a Question

30 mm Control Stations and Enclosures

Issue:
Can you provide the part number for the selector switch on a 9001BG112?

Product Line:
9001BG

Environment:
30mm Control Stations and Enclosures

Cause:
Assembly/wiring- Accessories

Resolution:
The selector switch is provided on the front cover plate. Consider the part number 9001BGC114. If the terminal blocks are required, consider the part number 9001BGB114.
Was this helpful?
What can we do to improve the information ?