Technical FAQs

Ask a Question

What does the CFI code indicate on the ATS48?

Issue:
CFI code on the display

Product Line:
ATS48

Environment:
All models and serial numbers.

Cause:
A CFI fault appears if an invalid configuration is loaded into the soft start.  Once a valid configuration is loaded into the soft start, this fault will clear itself.

Resolution:
Disable incompatible functions or values outside of the range of a parameter.
Recheck the programming and load a compatible configuration.
Was this helpful?
What can we do to improve the information ?