Technical FAQs

Ask a Question

Two-level float switch


Is there a two-level float switch

Product Line:

9038 float switches


US product


Two-level units are necessary for certain applications


The Form N4 added to certain 9038 float switches will change their function from an alternating unit to a two-level unit.  This form is not available on every model 9038.  Care should be taken to check availability before quotations are made.

Was this helpful?
What can we do to improve the information ?