Technical FAQs

Ask a Question

H3 contact arrangement

Issue:

What contact arrangement is signified by an H3 form code?

Product Line:

9001SK/9001K operators

Environment:

US Product

Cause:

Customers sometimes specify this contact arrangement

Resolution:

H3 signifies three 9001KA1 contact blocks attached to the operator.  Two will be stacked on the left and one will be on the right (facing the back of the operator).
 

Was this helpful?
What can we do to improve the information ?