Technical FAQs

Ask a Question

Vario & Mini-Vario Disconnect Switches

Issue:
What is the length of the shaft extension kit in the Mini-Vario Nema Type 1 & 12 Assembled Rear Mounting switch VCCDN20?

Product Line:
Mini-Vario & Vario Assembled and Enclosed switches.

Environment:
Mini-Vario & Vario UL 508 Disconnect Switches

Cause:
Assembly/wiring, Components

Resolution:
Please note that these shaft extension kits can be field modified to accommodate the depth of the panel. The two shafts extension kits for the VCCDN20 are listed below
Door To Panel Distance:         VZN17            300 - 330mm (min - max)
VZN30            400 - 430mm (min - max).
Was this helpful?
What can we do to improve the information ?