Technical FAQs

Ask a Question

Resetting a 2510M manual starter

Issue:

Will the 2510M manual starter automatically reset after it trips?

Product Line:

2510M manual starters

Environment:

US Product

Cause:

Some non-manual restarters are capable of auto resetting

Resolution:

No, this device must be physically reset by pressing in the stop/reset button all the way.
 

Was this helpful?
What can we do to improve the information ?