Technical FAQs

Ask a Question

G style mounting plate


What can be done to replace 9007TUG style limit switches

Product Line:

9007TUG limit switches


US Product only


The G mounting plate has been discontinued


The G style mounting plate was dimensionally equivalent to a D style mounting plate.  The difference between the two is that the G style had a cutout opening in it allowing wiring to pass through the plate.  The D style does not have this opening.  One can use the D style for equivalent mounting positions, but would have to either allow wiring to pass through the bottom of the switch or drill a hole in the plate to accomodate it instead.

Dimensional Drawing attached

Was this helpful?
What can we do to improve the information ?