Technical FAQs

Ask a Question

Can you set up the ATV61 and ATV71 drives to follow a 0 to 5vdc voltage signal?

Issue:
Can you set up the ATV61 and ATV71 drives to follow a 0 to 5vdc voltage signal?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Needs the drives AI2 voltage input to follow 0 to 5vdc not 0 to 10vdc.

Resolution:
Yes you can program the drive to do this function.
Programming assistance as follows
Go into Menu 1.5 Inputs and outputs
Go into AI2 configuration
Go into AI2 type is voltage
Go into AI2 min value is 0vd
Go into AI2 max value is 5vdc
 
Was this helpful?
What can we do to improve the information ?