Technical FAQs

Ask a Question

What is the replacement melting alloy overload relay for 8536 Type SA starter?

Issue:
What is the replacement melting alloy overload relay for 8536 Type SA starter?

Product Line:
Class 9065 Melting Alloy Overload Relays

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
The replacement melting alloy overload relay for a NEMA size 00

for single phase applications: 9065SDO4

for 3 phase applications: 9065SDO5
Was this helpful?
What can we do to improve the information ?