Technical FAQs

Ask a Question

Does the Powerpact MGA and MJA fit in the same space as the I-Line MA and MH breakers?

Issue:
Does the Powerpact MGA and MJA fit in the same space as the I-Line MA and MH breakers?

Product Line:
I-Line, Powerpact circuit breakers, Square D circuit breakers

Cause:
Need to replace existing legacy breakers

Resoluton:
The Powerpact M frame breakers are designed to fit in the same space as the legacy MA and MH breaker in I-Line panel. Both breaker types take 9 inches of mounting height and fit on the wide side of an I-Line distribution. The breakers fit in HCW, HCP, and HCR  I-Line panelboards.
Was this helpful?
What can we do to improve the information ?