Technical FAQs

Ask a Question

What are the dimensions for a NEMA 1 enclosure for a 8903 Type LXG?

Issue:
What are the dimensions for a NEMA 1 enclosure for a 8903 Type LXG?

Product Line:
8903 Type LG Lighting Contactors

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:

Width: 7.81 in. / 198 cm

Height: 12.69 in. / 322 cm

Depth: 6.03 in. / 153 cm
Was this helpful?
What can we do to improve the information ?