Technical FAQs

Ask a Question

Can more than one keypad be connected to an ATV312 drive?

Issue:
Customer wants to use three keypads at different locations and a modbus hub to split the connection.

Product line:
ATV312, Altivar 312, ATV12, Altivar 12

Environment:
All models

Cause:
n/a

Resolution:
The ATV312 can only have one remote connected at a time.  It is not possible to connect a splitter to use multiple remotes at the same time.
Was this helpful?
What can we do to improve the information ?