Technical FAQs

Ask a Question

Protection Rating for GV2E01

Issue:

What rating does the GV2E01 give when used with the GV2MC01 or GV2MP01 enclosure

Product Line:

GV2 Enclosure Accessories

Environment:

US Product

Cause:

The IP rating is not specified in the Digest 176

Resolution:

When used with the GV2MC01 or GV2MP01, this kit will give a IP55 rating

Was this helpful?
What can we do to improve the information ?