Technical FAQs

Ask a Question

What is the pick-up time for a 8430MP Phase Failure relay

Issue:
Clarify the pick-up time for 8430MP Phase Failure relay

Product Line:
Supervisory Relays Type M- Phase failure for 3 Phase Monitoring.

Environment:
Phase Failure And Under-voltage Relay 8430MPSV24, 8430MPSV29, voltage relay phase failure loss reversal under over 480v volts 3-phase shunt trip   Relays / Timers

Cause:
Need to confirm pick-up time for a specific application

Resolution:
When the correct 3 phase voltage is applied, typically 0.1 seconds. 
 
Was this helpful?
What can we do to improve the information ?