Technical FAQs

Ask a Question

What is the standard amp range for a NEMA size 5 solid state overload?

Issue:
What is the standard amp range for a NEMA size 5 solid state overload?

Product Line:
Class 9065 Solid State Overload Relays

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
The standard amp range is 90-270A
Was this helpful?
What can we do to improve the information ?