Technical FAQs

Ask a Question

Can a low voltage switch be used to trigger the relay of a Power Pack SLSPP1277?

Issue:
Customer would like to use a switch device to trigger a Power Pack Relay.  Is this permissible and how can it be done?  

Product Line:
Lighting Control Occupancy Sensors
SLSPP1277 SLSPP1347  

Environment:
Commercial Lighting Control

Cause:
The Power Pack is normally wired to an SLS-series Occupancy Sensor.  The customer would like to use the Power Pack without an occupancy sensor and trigger it by another external switch device instead.

Resolution:
Trigger the Power Pack relay by connecting the low voltage Red wire to the blue wire with a dry contact closure.  This closure will cause the red wire on the line voltage side of the Power Pack to be energized.




 
Was this helpful?
What can we do to improve the information ?