Technical FAQs

Ask a Question

What is a 'Virtual Main' and how do I use it to reduce Arc Flash Incident Energy?

A virtual Main consists of a digital relay and CT's added to the LV side of a substation transformer and wired to a Fault Breaking overcurrent device (Vacuum C/B) with the ability to use a "Maintenance Switch" to set a lower fault level trip or to use Short time Zone interlocking with the Secondary feeders to allow for faster tripping of the "virtual" main. 
 
Was this helpful?
What can we do to improve the information ?