Technical FAQs

Ask a Question

What size Hubs are needed for 8538SCW NEMA 4/4X enclosure?

Issue:
What size Hubs are needed for 8538SCW NEMA 4/4X enclosure?

Product Line:
NEMA 4 & 4X Enclosures

Environment:
US Product Lines

Cause:
The enclosure drawing on EWay does not specify

Resolution:
There are two Hubs needed for the bottom, 3/4" and 1" Hubs, and one 1" Hub for the top.
Was this helpful?
What can we do to improve the information ?